cancel
Showing results for 
Search instead for 
Did you mean: 

WB55: Sleep current too high

G5658
Associate II

I tried flashing PWR_STANDBY_RTC and PWR_EnterStandbyMode examples both has sleep current of 590uA. How do i get the datasheet value of 600nA standby current or atleast something less than 10uA.

1 ACCEPTED SOLUTION

Accepted Solutions
G5658
Associate II

It seems once flashing is done, i need to remove the jumper in JP5 that connects VDD to T_VDD or else the level shifter will burn 600uA+ of current.

View solution in original post

3 REPLIES 3
G5658
Associate II

Shouldn't current be measured at JP3 and not JP2?

Peter BENSCH
ST Employee

Well, JP3 and JP2 are connected in series, so either one would make the measurement of the current consumption possible.

JP3 relates to the VDD of the WB55, while JP2 also includes VDDSMPS.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
G5658
Associate II

It seems once flashing is done, i need to remove the jumper in JP5 that connects VDD to T_VDD or else the level shifter will burn 600uA+ of current.