2023-02-22 04:23 AM
We have a design implementing the STM32WL55/WE5.
The recommended crystals on the reference designs and literature are:
NX2012SA 32.768KHz EXS00A-MU00527X2
NX2016SA 32MHz EXS00A-CS06465
I want to verify that it is OK to use the following:
For NX2016SA: EIIECS-320-10-37B-CKY-TR
CRYSTAL 32.0000MHZ 10PF SMD ESR 50 ±10ppm ±10ppm -30 ~ 85 2.0x1.6x0.45mm
For NT2016SF-32M-END5875A: EIIECS-TXO-20CSMV-320-EY-TR
MultiVoltTCXO,32MHz,±2.5ppm,1.7V~3.465V,2.5mA,-30°C~85°C,ClippedSineWave
The design must comply with SigFox and LoRa spec and will potentially be in field for a long time (10+ years).
Datasheets attached.
2023-02-22 09:36 AM
Hello @DRoss.3 and welcome to the Community 🙂
For information about crystal compatibility with STM32WLSeries, please refer to the AN5042 and
Table 7. Recommended crystal / MEMS resonators for the LSE oscillator in STM32 products (in AN2867)
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen