cancel
Showing results for 
Search instead for 
Did you mean: 

Verification of Crystal suitability for STM32WL design

DRoss.3
Associate

We have a design implementing the STM32WL55/WE5.

The recommended crystals on the reference designs and literature are:

NX2012SA 32.768KHz EXS00A-MU00527X2

NX2016SA 32MHz EXS00A-CS06465

I want to verify that it is OK to use the following:

For NX2016SA:  EIIECS-320-10-37B-CKY-TR

CRYSTAL 32.0000MHZ 10PF SMD ESR 50 ±10ppm ±10ppm -30 ~ 85 2.0x1.6x0.45mm

For NT2016SF-32M-END5875A:  EIIECS-TXO-20CSMV-320-EY-TR

MultiVoltTCXO,32MHz,±2.5ppm,1.7V~3.465V,2.5mA,-30°C~85°C,ClippedSineWave

The design must comply with SigFox and LoRa spec and will potentially be in field for a long time (10+ years).

Datasheets attached.

1 REPLY 1
Imen.D
ST Employee

Hello @DRoss.3​ and welcome to the Community :)

For information about crystal compatibility with STM32WLSeries, please refer to the AN5042 and

Table 7. Recommended crystal / MEMS resonators for the LSE oscillator in STM32 products (in AN2867)

0693W00000aHRfTQAW.png 

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen