2018-05-22 3:32 AM
Hello everyone,
This is my first post here.
As part of my research with LoRaWAN, I am working on a custom built board having an STM32L072 module. One of the critical sections of my research involves calculating the energy consumption during transmission and reception. Hence I am looking for a method to power the board using 3.3v and log the voltage and current consumption.
As so I came across X-NUCLEO-LPM01A. According to its datasheet:
'It can be used to supply and measure the consumption of STM32 Nucleo-32, Nucleo-64 or Nucleo-144 boards, using Arduino connectors. Alternatively, it supplies and measures the consumption of any target connected by wires via the basic connector.'
My custom built board simply needs a VCC and a GND to operate. So I was wondering if
X-NUCLEO-LPM01A will suffice for this project. I was not able to find any video demonstrating the same.
Please advice.
Thanks
Sujan.
#power-measurement #stm32l072 #lorawan #x-nucleo-lpm01a