Thread_Coap_MultiBoard more steps to enable traces over uart ?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-04-01 02:44 AM
Hi everyone,
I started to work with the "Thread_Coap_MultiBoard" example , all work fine , but now i want to display the traces over RS232.
4) Activate the traces if necessary:
=====================================
If you want to get the traces in real time, you can connect an HyperTerminal
via an UART RS232 cable using the following connections:
RXD: CN10(Pin35)
TXD: CN10(Pin37)
For the traces, the UART must be configured as follows:
- BaudRate = 115200 baud
- Word Length = 8 Bits
- Stop Bit = 1 bit
- Parity = none
- Flow control = none
* <h3><center>© COPYRIGHT STMicroelectronics</center></h3>
*/
app_conf.h
* Note : Refer to utilities_conf.h file in order to details
* the level of traces : CFG_DEBUG_TRACE_FULL or CFG_DEBUG_TRACE_LIGHT
*****************************************************************************/
#define CFG_DEBUG_TRACE 1
following the readme file the traces should be already enabled, but i got nothing in the terminal, so maybe there is more steps to achieve this ?
regards,
Pierre
Labels:
- Labels:
-
STM32WB series
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-04-02 05:15 AM
up !
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-04-06 03:09 AM
UP