2021-07-12 06:57 PM
In my testing, I programmed two NUCELO-WL55JC2's to communicate with one another. I found that I could only receive if the transmitter antenna was aligned and touching the receiving antenna.
After further debugging, I traced the issue to the LPO.
Using the low power output (even at +15dBm), gave greatly attentuated transmissions. The two antennas had to be touching.
On the other hand, using the high power output (even at only +14dBm), I could transmit at range.
Have I missed a setting for transmission? My process was based on RM0461.
2023-02-16 09:22 AM
Hi MAfri.1,
I have the same issue. I can only get the two to talk to each other using the ping pong example if the antennas are touching or almost touching. If I have them even just 4 inches away they will struggle to match CRC. Did you ever figure out this issue?
Thanks,
Corey