cancel
Showing results for 
Search instead for 
Did you mean: 

SWD and BOOT Pin lockout - STM32WL33

CEagl.1
Associate III

Hello,

I am looking to add an STDC14 header to my design.
I am concerned that by putting such a connector on the board, this will allow 3rd parties to simply buy an STLINK and reprogram my device.

I am not familiar with STM32, so in the interest of speed, can anyone tell me if the SWD and BOOT pins can be disabled following an initial programming?

If not is there a method of protecting these pins from 3rd parties?

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

See RM0511, section 9.3.6: Size register (SIZE), where you can disable SWD (bit 20).

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

See RM0511, section 9.3.6: Size register (SIZE), where you can disable SWD (bit 20).

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.