2023-07-18 06:17 AM
Hi All,
I'm using STM32WL55JC board which include Sub-GHz, ADC and DMA peripherals (and many more of course)
I run "ping pong" example to create Sub-GHz communication sucssfully, also run "ADC_SingleConversion_TriggerTimer_DMA" and changed to circular mode (DMA) I saw buffer changing variables according to ADC result.
I configured ADC and DMA at "ping pong" example exactly as they configured at ADC example, and start via HAL_ADC_Start_DMA() command the buffer result is written only once, then program start Sub_GHz routine of RX-TX and the buffer results stuck and doesn't change.
what can be the reason?
adding some pictures from ping-pong - ADC DMA configuration
I'll appreciate your help!
2023-07-18 06:24 AM
I think you should provide the code, instead of the screenshots.
2023-07-18 06:29 AM
ON SUB-GHZ-INIT ADC_DMA START
******************************************************************************
* @file subghz_phy_app.c
* @author MCD Application Team
* @brief Application of the SubGHz_Phy Middleware
******************************************************************************
* @attention
*
* Copyright (c) 2021 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "platform.h"
#include "sys_app.h"
#include "subghz_phy_app.h"
#include "radio.h"
#include "adc.h"
#include "stdio.h"
#include "stdlib.h"
#include "ctype.h"
/* USER CODE BEGIN Includes */
#include "stm32_timer.h"
#include "stm32_seq.h"
#include "utilities_def.h"
#include "app_version.h"
#include "subghz_phy_version.h"
/* USER CODE END Includes */
/* External variables ---------------------------------------------------------*/
/* USER CODE BEGIN EV */
/* USER CODE END EV */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
typedef enum
{
RX,
RX_TIMEOUT,
RX_ERROR,
TX,
TX_TIMEOUT,
} States_t;
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* Configurations */
/*Timeout*/
#define RX_TIMEOUT_VALUE 3000
#define TX_TIMEOUT_VALUE 3000
#define PWMSettleTime 1000 //one second
/* PING string*/
#define SYNC "SYNC"
#define SYNCRESPONSE "SYNC2 DONE"
#define ID "NODE1B"
#define COMMA ","
/*Size of the payload to be sent*/
/* Size must be greater of equal the PING and PONG*/
#define MAX_APP_BUFFER_SIZE 255
#if (PAYLOAD_LEN > MAX_APP_BUFFER_SIZE)
#error PAYLOAD_LEN must be less or equal than MAX_APP_BUFFER_SIZE
#endif /* (PAYLOAD_LEN > MAX_APP_BUFFER_SIZE) */
/* wait for remote to be in Rx, before sending a Tx frame*/
#define RX_TIME_MARGIN 200
/* Afc bandwidth in Hz */
#define FSK_AFC_BANDWIDTH 83333
/* LED blink Period*/
#define LED_PERIOD_MS 200
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
static void MX_DMA_Init(void);
/* Private variables ---------------------------------------------------------*/
/* Radio events function pointer */
static RadioEvents_t RadioEvents;
/* USER CODE BEGIN PV */
/*Ping Pong FSM states */
static States_t State = RX;
/* App Rx Buffer*/
static uint8_t BufferRx[MAX_APP_BUFFER_SIZE];
/* App Tx Buffer*/
static uint8_t BufferTx[MAX_APP_BUFFER_SIZE];
/* Last Received Buffer Size*/
uint16_t RxBufferSize = 0;
/* Last Received packer Rssi*/
int8_t RssiValue = 0;
/* Last Received packer SNR (in Lora modulation)*/
int8_t SnrValue = 0;
/* Led Timers objects*/
static UTIL_TIMER_Object_t timerLed;
/* device state. Master: true, Slave: false*/
bool isMaster = true;
/* random delay to make sure 2 devices will sync*/
/* the closest the random delays are, the longer it will
take for the devices to sync when started simultaneously*/
static int32_t random_delay;
extern ADC_HandleTypeDef hadc;
#define ADC_CONVERTED_DATA_BUFFER_SIZE ((uint32_t) 200 )
__IO uint16_t aADCxConvertedData[ADC_CONVERTED_DATA_BUFFER_SIZE]; /* ADC group regular conversion data (array of data) */
/* Variables for ADC conversion data */
//__IO uint16_t uhADCxConvertedData = VAR_CONVERTED_DATA_INIT_VALUE; /* ADC group regular conversion data */
#define DIGITAL_SCALE_12BITS ((uint32_t) 0xFFF)
/* Init variable out of ADC expected conversion data range */
#define VAR_CONVERTED_DATA_INIT_VALUE (DIGITAL_SCALE_12BITS + 1)
/* Variables for ADC conversion data computation to physical values */
uint16_t uhADCxConvertedData_Voltage_mVolt [ADC_CONVERTED_DATA_BUFFER_SIZE]; /* Value of voltage calculated from ADC conversion data (unit: mV) */
unsigned long value = 0;
#define NumberOfPeaksRequired ((uint32_t) 3)
volatile uint16_t MaxPeak = 0 ;
volatile uint16_t ArrayMaxPeakmV [NumberOfPeaksRequired];
volatile uint16_t i = 0;
volatile uint16_t NumberOfMaxPeak = 0;
volatile double AverageMaxPeakmV = 0;
__IO uint16_t uhADCxConvertedData = VAR_CONVERTED_DATA_INIT_VALUE; /* ADC group regular conversion data */
int8_t IDNumber = 2;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
/*!
* @brief Function to be executed on Radio Tx Done event
*/
static void OnTxDone(void);
/**
* @brief Function to be executed on Radio Rx Done event
* @PAram payload ptr of buffer received
* @PAram size buffer size
* @PAram rssi
* @PAram LoraSnr_FskCfo
*/
static void OnRxDone(uint8_t *payload, uint16_t size, int16_t rssi, int8_t LoraSnr_FskCfo);
/**
* @brief Function executed on Radio Tx Timeout event
*/
static void OnTxTimeout(void);
/**
* @brief Function executed on Radio Rx Timeout event
*/
static void OnRxTimeout(void);
/**
* @brief Function executed on Radio Rx Error event
*/
static void OnRxError(void);
/* USER CODE BEGIN PFP */
/**
* @brief Function executed on when led timer elapses
* @PAram context ptr of LED context
*/
static void OnledEvent(void *context);
/**
* @brief PingPong state machine implementation
*/
static void PingPong_Process(void);
bool isIDPresentInBuffer(const char *id);
/* USER CODE END PFP */
/* Exported functions ---------------------------------------------------------*/
void SubghzApp_Init(void)
{
/* USER CODE BEGIN SubghzApp_Init_1 */
MX_ADC_Init();
MX_DMA_Init();
HAL_ADC_Start_DMA(&hadc,
(uint32_t *)aADCxConvertedData,
ADC_CONVERTED_DATA_BUFFER_SIZE
);
APP_LOG(TS_OFF, VLEVEL_M, "\n\rPING PONG\n\r");
/* Get SubGHY_Phy APP version*/
APP_LOG(TS_OFF, VLEVEL_M, "APPLICATION_VERSION: V%X.%X.%X\r\n",
(uint8_t)(APP_VERSION_MAIN),
(uint8_t)(APP_VERSION_SUB1),
(uint8_t)(APP_VERSION_SUB2));
/* Get MW SubGhz_Phy info */
APP_LOG(TS_OFF, VLEVEL_M, "MW_RADIO_VERSION: V%X.%X.%X\r\n",
(uint8_t)(SUBGHZ_PHY_VERSION_MAIN),
(uint8_t)(SUBGHZ_PHY_VERSION_SUB1),
(uint8_t)(SUBGHZ_PHY_VERSION_SUB2));
/* Led Timers*/
UTIL_TIMER_Create(&timerLed, LED_PERIOD_MS, UTIL_TIMER_ONESHOT, OnledEvent, NULL);
UTIL_TIMER_Start(&timerLed);
/* USER CODE END SubghzApp_Init_1 */
/* Radio initialization */
RadioEvents.TxDone = OnTxDone;
RadioEvents.RxDone = OnRxDone;
RadioEvents.TxTimeout = OnTxTimeout;
RadioEvents.RxTimeout = OnRxTimeout;
RadioEvents.RxError = OnRxError;
Radio.Init(&RadioEvents);
/* USER CODE BEGIN SubghzApp_Init_2 */
/*calculate random delay for synchronization*/
random_delay = (Radio.Random()) >> 22; /*10bits random e.g. from 0 to 1023 ms*/
/* Radio Set frequency */
Radio.SetChannel(RF_FREQUENCY);
/* Radio configuration */
#if ((USE_MODEM_LORA == 1) && (USE_MODEM_FSK == 0))
APP_LOG(TS_OFF, VLEVEL_M, "---------------\n\r");
APP_LOG(TS_OFF, VLEVEL_M, "LORA_MODULATION\n\r");
APP_LOG(TS_OFF, VLEVEL_M, "LORA_BW=%d kHz\n\r", (1 << LORA_BANDWIDTH) * 125);
APP_LOG(TS_OFF, VLEVEL_M, "LORA_SF=%d\n\r", LORA_SPREADING_FACTOR);
Radio.SetTxConfig(MODEM_LORA, 22, 0, LORA_BANDWIDTH,
LORA_SPREADING_FACTOR, LORA_CODINGRATE,
LORA_PREAMBLE_LENGTH, LORA_FIX_LENGTH_PAYLOAD_ON,
true, 0, 0, LORA_IQ_INVERSION_ON, TX_TIMEOUT_VALUE);
Radio.SetRxConfig(MODEM_LORA, LORA_BANDWIDTH, LORA_SPREADING_FACTOR,
LORA_CODINGRATE, 0, LORA_PREAMBLE_LENGTH,
LORA_SYMBOL_TIMEOUT, LORA_FIX_LENGTH_PAYLOAD_ON,
0, true, 0, 0, LORA_IQ_INVERSION_ON, true);
Radio.SetMaxPayloadLength(MODEM_LORA, MAX_APP_BUFFER_SIZE);
#elif ((USE_MODEM_LORA == 0) && (USE_MODEM_FSK == 1))
APP_LOG(TS_OFF, VLEVEL_M, "---------------\n\r");
APP_LOG(TS_OFF, VLEVEL_M, "FSK_MODULATION\n\r");
APP_LOG(TS_OFF, VLEVEL_M, "FSK_BW=%d Hz\n\r", FSK_BANDWIDTH);
APP_LOG(TS_OFF, VLEVEL_M, "FSK_DR=%d bits/s\n\r", FSK_DATARATE);
Radio.SetTxConfig(MODEM_FSK, TX_OUTPUT_POWER, FSK_FDEV, 0,
FSK_DATARATE, 0,
FSK_PREAMBLE_LENGTH, FSK_FIX_LENGTH_PAYLOAD_ON,
true, 0, 0, 0, TX_TIMEOUT_VALUE);
Radio.SetRxConfig(MODEM_FSK, FSK_BANDWIDTH, FSK_DATARATE,
0, FSK_AFC_BANDWIDTH, FSK_PREAMBLE_LENGTH,
0, FSK_FIX_LENGTH_PAYLOAD_ON, 0, true,
0, 0, false, true);
Radio.SetMaxPayloadLength(MODEM_FSK, MAX_APP_BUFFER_SIZE);
#else
#error "Please define a modulation in the subghz_phy_app.h file."
#endif /* USE_MODEM_LORA | USE_MODEM_FSK */
/*fills tx buffer*/
//memset(BufferTx, 0x0, MAX_APP_BUFFER_SIZE);
APP_LOG(TS_ON, VLEVEL_L, "rand=%d\n\r", random_delay);
/*starts reception*/
Radio.Rx(RX_TIMEOUT_VALUE + random_delay);
/*register task to to be run in while(1) after Radio IT*/
UTIL_SEQ_RegTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), UTIL_SEQ_RFU, PingPong_Process);
/* USER CODE END SubghzApp_Init_2 */
}
/* USER CODE BEGIN EF */
/* USER CODE END EF */
/* Private functions ---------------------------------------------------------*/
static void OnTxDone(void)
{
/* USER CODE BEGIN OnTxDone */
APP_LOG(TS_ON, VLEVEL_L, "OnTxDone\n\r");
/* Update the State of the FSM*/
State = TX;
/* Run PingPong process in background*/
UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
/* USER CODE END OnTxDone */
}
static void OnRxDone(uint8_t *payload, uint16_t size, int16_t rssi, int8_t LoraSnr_FskCfo)
{
/* USER CODE BEGIN OnRxDone */
APP_LOG(TS_ON, VLEVEL_L, "OnRxDone\n\r");
#if ((USE_MODEM_LORA == 1) && (USE_MODEM_FSK == 0))
APP_LOG(TS_ON, VLEVEL_L, "I'm $ %s $ Recieved this data $ %s $ RssiValue=%d dBm, SnrValue=%ddB\n\r", ID , BufferRx , rssi, LoraSnr_FskCfo); /* Record payload Signal to noise ratio in Lora*/
SnrValue = LoraSnr_FskCfo;
#endif /* USE_MODEM_LORA | USE_MODEM_FSK */
#if ((USE_MODEM_LORA == 0) && (USE_MODEM_FSK == 1))
APP_LOG(TS_ON, VLEVEL_L, "RssiValue=%d dBm, Cfo=%dkHz\n\r", rssi, LoraSnr_FskCfo);
SnrValue = 0; /*not applicable in GFSK*/
#endif /* USE_MODEM_LORA | USE_MODEM_FSK */
/* Update the State of the FSM*/
State = RX;
/* Clear BufferRx*/
memset(BufferRx, 0, MAX_APP_BUFFER_SIZE);
/* Record payload size*/
RxBufferSize = size;
if (RxBufferSize <= MAX_APP_BUFFER_SIZE)
{
memcpy(BufferRx, payload, RxBufferSize);
}
/* Record Received Signal Strength*/
RssiValue = rssi;
/* Record payload content*/
APP_LOG(TS_ON, VLEVEL_H, "payload. size=%d \n\r", size);
for (int32_t i = 0; i < PAYLOAD_LEN; i++)
{
APP_LOG(TS_OFF, VLEVEL_H, "%02X", BufferRx[i]);
if (i % 16 == 15)
{
APP_LOG(TS_OFF, VLEVEL_H, "\n\r");
}
}
APP_LOG(TS_OFF, VLEVEL_H, "\n\r");
/* Run PingPong process in background*/
UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
/* USER CODE END OnRxDone */
}
static void OnTxTimeout(void)
{
/* USER CODE BEGIN OnTxTimeout */
APP_LOG(TS_ON, VLEVEL_L, "OnTxTimeout\n\r");
/* Update the State of the FSM*/
State = TX_TIMEOUT;
/* Run PingPong process in background*/
UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
/* USER CODE END OnTxTimeout */
}
static void OnRxTimeout(void)
{
/* USER CODE BEGIN OnRxTimeout */
APP_LOG(TS_ON, VLEVEL_L, "OnRxTimeout\n\r");
/* Update the State of the FSM*/
State = RX_TIMEOUT;
/* Run PingPong process in background*/
UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
/* USER CODE END OnRxTimeout */
}
static void OnRxError(void)
{
/* USER CODE BEGIN OnRxError */
APP_LOG(TS_ON, VLEVEL_L, "OnRxError\n\r");
/* Update the State of the FSM*/
State = RX_ERROR;
/* Run PingPong process in background*/
UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), CFG_SEQ_Prio_0);
/* USER CODE END OnRxError */
}
/* USER CODE BEGIN PrFD */
static void PingPong_Process(void)
{
Radio.Sleep();
switch (State)
{
case RX:
if (RxBufferSize > 0)
{
if (strncmp((const char *)BufferRx, SYNC, sizeof(4)) == 0)
{
// Search for ID in the line
// SOME CODE TBD
}
else if (strncmp((const char *)BufferRx, ID, sizeof(ID) - 1 ) == 0)
{
for (i = 0 ; i <= ADC_CONVERTED_DATA_BUFFER_SIZE ; i++ )
{
//Search for the max peak value
if (MaxPeak < aADCxConvertedData[i] )
{
//Insert peak value to
MaxPeak = aADCxConvertedData[i];
}
}
UTIL_TIMER_Stop(&timerLed);
/* switch off red led */
HAL_GPIO_WritePin(LED3_GPIO_Port, LED3_Pin, GPIO_PIN_RESET); /* LED_RED */
/* slave toggles green led */
HAL_GPIO_TogglePin(LED2_GPIO_Port, LED2_Pin); /* LED_GREEN */
/* Add delay between RX and TX */
//HAL_Delay(Radio.GetWakeupTime() );//HAL_Delay(Radio.GetWakeupTime() + RX_TIME_MARGIN);
/*slave sends PONG*/
APP_LOG(TS_ON, VLEVEL_L, "Slave Tx start\n\r");
APP_LOG(TS_ON, VLEVEL_L,
"Yay you call me 🙂 %s So take my data %d \n \r" ,(const char *) ID ,MaxPeak ,
"\n\r");
memcpy(BufferTx, ID, sizeof(ID));
sprintf(BufferTx, "%s%s%d",ID , COMMA , MaxPeak);
Radio.Send(BufferTx, PAYLOAD_LEN);
//NVIC_SystemReset();
}
else /* valid reception but not a PING as expected */
{
APP_LOG(TS_ON, VLEVEL_L, "No this node, I received the following address of node %s\n\r" , (const char *)BufferRx);
Radio.Rx(RX_TIMEOUT_VALUE);
}
}
break;
case TX:
APP_LOG(TS_ON, VLEVEL_L, "Rx start\n\r");
Radio.Rx(RX_TIMEOUT_VALUE);
break;
case RX_TIMEOUT:
case RX_ERROR:
APP_LOG(TS_ON, VLEVEL_L, "Slave Rx start\n\r");
Radio.Rx(RX_TIMEOUT_VALUE);
break;
case TX_TIMEOUT:
APP_LOG(TS_ON, VLEVEL_L, "Slave Rx start\n\r");
Radio.Rx(RX_TIMEOUT_VALUE);
break;
default:
break;
}
}
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMAMUX1_CLK_ENABLE();
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Channel1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
}
static void OnledEvent(void *context)
{
HAL_GPIO_TogglePin(LED2_GPIO_Port, LED2_Pin); /* LED_GREEN */
HAL_GPIO_TogglePin(LED3_GPIO_Port, LED3_Pin); /* LED_RED */
UTIL_TIMER_Start(&timerLed);
}
2023-07-18 07:23 AM
Short explanation:
I have 2 boards, I want that every board will start ADC and measure specific channel and configured this channel, the channel initialize at "subghz_phy_app.c"(the code above) and also start ADC_DMA at SubghzApp_Init()
from buffer of 200 ADC values I'm looking for max value and send it Sub-GHz, after sending it I want to find new max from new buffer ADC results, but I always get the same value (although I change ADCin via external P.S.)
meaning that buffer values doesn't change