2025-02-13 10:50 PM
Hi,
I'm doing tests based on the LoRaWAN_AT_Slave. One of the modules often appears tMAC txTimeOut, resulting in JOIN FAILED. Same firmware downloaded, but some devices are working, is there any doubt? Is it a hardware problem?
[14:47:35.933]发→◇AT+JOIN=1
□
[14:47:35.965]收←◆1s890:TX on freq 470900000 Hz at DR 0
OK
[14:47:39.965]收←◆5s893:MAC txTimeOut
+EVT:JOIN FAILED
Solved! Go to Solution.
2025-02-21 12:39 AM
Hi,
I have finally solved the problem, it is the hardware cause.
Thanks.
2025-02-14 1:20 PM - edited 2025-02-14 1:21 PM
Hello @ethan2
Could you please provide more details. What is the exact module you are using (a third party module or a module based on your own design), what is the code you are using and all your use case details if possible.
Best Reagards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-21 12:39 AM
Hi,
I have finally solved the problem, it is the hardware cause.
Thanks.