cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WL33 with LoRa

Erlkoenig
Associate III

Hi,

I have seen that the new STM32WL33 have support for 4-FSK, high receive sensitivity and wake-up receiver LPAWUR, which is beneficial for both high-data-rate and long-range applications. However, LoRa support is reserved for STM32WL55 and STM32WLE5, which don't support 4-FSK.

Will there be a controller that combines both LoRa and also 4-FSK support, and perhaps also higher sensitivity and LPAWUR?

Thank you very much!

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Erlkoenig and welcome to the ST Community :smiling_face_with_smiling_eyes:.

For now, there is no release that support all those features on the same SOC. If you are looking for such product for specific needs, you can contact our local FAEs or sales and marketing offices for such a purpose.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @Erlkoenig and welcome to the ST Community :smiling_face_with_smiling_eyes:.

For now, there is no release that support all those features on the same SOC. If you are looking for such product for specific needs, you can contact our local FAEs or sales and marketing offices for such a purpose.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi, thank you very much for your reply!


@@STTwo-3 wrote:

If you are looking for such product for specific needs, you can contact our local FAEs or sales and marketing offices for such a purpose.


 

Thanks, I will consider this.