2026-01-21 1:52 AM - last edited on 2026-03-02 7:24 AM by Imen.D
Hello There
i am using https://github.com/STMicroelectronics/STM32CubeWL/tree/main/Projects/NUCLEO-WL55JC/Applications/LoRaWAN/LoRaWAN_End_Node_FreeRTOS this example ,
in that there is timer used for sent the data , i want RTC for send data for particular time and all how can i do ???
2026-01-21 1:59 AM
I would start by looking at examples to use the RTC.
Get one/some of them working to understand the RTC.
Also read the Reference Manual section on the RTC.
See also Application Note AN4759, "Introduction to using the hardware real-time clock (RTC) and the tamper management unit (TAMP) with STM32 MCUs"
via: https://www.st.com/en/microcontrollers-microprocessors/stm32wl55jc.html#documentation
2026-01-21 2:01 AM
in the example of FreeRTOS_End_Node i am unable to initialize RTC if you provide me example for that its very good for me
2026-01-21 2:12 AM
Before trying to add it to some other project, have you got it working in a simple, standalone example?
Always best to start simple to gain understanding.
Once you've got that, you'll have a working example for reference ...
2026-01-21 2:16 AM
Actually in Lorawan_end_Node_freertos example the RTC is conflicting with UTIL TImer so
Standalone works
2026-01-21 2:26 AM
So what is the conflict?