2026-01-20 1:52 AM - last edited on 2026-03-02 7:23 AM by Imen.D
Hi,
I'm using a STM32WL5MOC. I see that in the LoRaWAN_Init the LmHandlerJoin is not in a USER CODE section, meaning that it can't be disabled. In my application I would like to do the join upon my request and not in the init. How I can prevent from join?
/* USER CODE END LoRaWAN_Init_2 */
LmHandlerJoin(ActivationType, ForceRejoin);
if (EventType == TX_ON_TIMER)
Thanks.
2026-01-21 3:55 PM
I haven't tried this specific case, but you might be able to change this in CubeMX:
2026-01-22 1:07 AM
Thanks @Dana Myers. I think that "Force rejoin at each reboot" prevent only a new join if you have already restored the NVM context. Infact, in lora_app.h there is a comment on the variable:
/*!
* LoRaWAN force rejoin even if the NVM context is restored
* @note useful only when context management is enabled by CONTEXT_MANAGEMENT_ENABLED
*/
#define LORAWAN_FORCE_REJOIN_AT_BOOT true