2023-08-21 9:49 AM
Hi, I'm using STM32WLE5CCUx MCUs with STM32Cube FW_WL_V1.3.0 firmware package. In order to find a workaround to this issue I'm trying to set the uplink messages as CONFIRMED.
In this regard, once a MAC Tx_timeout is reached, is the re-transmission logic already implemented and executed by the middleware itself or do I have to explicitly build that logic in the app layer?
I tried to deduce the logic from the code but I couldn't have a good conclusion.
Thanks in advance!
2023-09-12 2:43 AM
On 1.0.3 link layer is't easy.
Set the parameter LmHandlerParams.IsTxConfirmed=LORAMAC_HANDLER_CONFIRMED_MSG; before send the pocket using the LmHandlerSend(); if the ack not receved the Stack will transmit the same packet for the number of times stored in this value MAX_ACK_RETRIES.
But if you are runing the 1.0.4 link layer then you have to hundle the retransmissions by your self, using the callback OnTxData().