Skip to main content
SWenn.1
Senior III
October 24, 2024
Solved

STM32WB5MMGH6 Project?

  • October 24, 2024
  • 1 reply
  • 562 views

Hello.

I have done a few projects in the past with the above module and am currently working on a motor controller project using an X-NUCLEO-IHM03A and an NUCLEO-F401.  I want to know if the STM32WB5MMHG6 has enough room and power to integrate the motor controller application into the STM32WB5MMHG6 M4 core ?  Has anyone done this or can anyone point me to information regarding this?

 

Thanks

This topic has been closed for replies.
Best answer by STTwo-32

Hello @SWenn.1 

The capability to use a STM32WB on a motor control project may depend on the application characteristics. There is an example demonstrating how to spin a gimbal motor using STM32WB55 and ST's MCSDK v6 sensorless six-step algorithm: WB55Gimbal-6steps

So, this should be possible depending on the application. You may can give more details on your application and create a new post on the motor control forum to view the if it is possible or not.

Best Regards.

STTwo-32

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
November 19, 2024

Hello @SWenn.1 

The capability to use a STM32WB on a motor control project may depend on the application characteristics. There is an example demonstrating how to spin a gimbal motor using STM32WB55 and ST's MCSDK v6 sensorless six-step algorithm: WB55Gimbal-6steps

So, this should be possible depending on the application. You may can give more details on your application and create a new post on the motor control forum to view the if it is possible or not.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.