2020-10-23 05:08 AM
Hi there,
I use the Nucleo-WB55 Board and I want to set some GPIO PINs in a high speed.
I use Low Level code to get fastest response.
GPIO_Init:
GPIO_InitStruct.Pin = PID_D0_Pin|PID_D1_Pin;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
LL_GPIO_Init(GPIOC, &GPIO_InitStruct);
The CubeMX clock setup is at maximum speed with 32MHz
I set/reset the GPIO with LL command at the main.c
LL_GPIO_ResetOutputPin(PID_D1_GPIO_Port,PID_D1_Pin); // time 0.00 µs
LL_GPIO_ResetOutputPin(PID_D0_GPIO_Port,PID_D0_Pin); // time 720 ns
It takes incredible 720ns until the D0 has turned off. It means there is a delay of 720ns until both Pin's D1 and D0 are off.
The LL_GPIO_ResetOutputPin() contains only WRITE_REG(GPIOx->BRR, PinMask);
Did anyone know the reason why the GPIO set/reset need this much time?
If I do the same with an old 8bit 14MHz MCU it takes only 140ns!
We want to replace the old 8bit MCU with the STM32wb to have Bluetooth. But if the GPIO can not run with the same speed as the old 8bit, we have to search for another MCU.
Thanks a lot for any idea to speed up the STM32wb.
Ferdi
Solved! Go to Solution.
2020-10-23 06:06 AM
If you want the fastest speed, use register level access. Ensure optimization settings are the highest.
GPIOD->BRR = GPIO_PIN_0 | GPIO_PIN_1;
You can examine the disassembly to see what code it's actually running.
2020-10-23 06:06 AM
If you want the fastest speed, use register level access. Ensure optimization settings are the highest.
GPIOD->BRR = GPIO_PIN_0 | GPIO_PIN_1;
You can examine the disassembly to see what code it's actually running.
2020-10-26 05:12 AM
Thank's this helps a lot. Both PIN's are set at the same time.
👍