cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 reference manual not available

LXu.4
Associate II

Does anyone use STM32WB55 now? The Reference Manuals is not available on this website.

Neither KEIL nor IAR seem to support the chip�?

4 REPLIES 4
Uwe Bonnes
Principal III

<sarcasme > Hey, it is only a year since the first announcement</sarcasme>.

Yes, we have been waiting for a year. Still no samples or evaluation boards were available�?

Amel NASRI
ST Employee

Hello,

There was an internal issue faced to publish the reference manual.

Now it is OK, the RM0434 is available on web.

Sorry for such inconvenience.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Le Corre Pierre
Associate III

Concerning the IDE:

For IAR, you can use the latest available version 8.32.3 with STM32WB product.

For Keil, you can download the associated pack

Version: 1.0.0 (2019-03-01) Keil.STM32WBxx_DFP.1.0.0.pack

Both of these version are compatible with the examples provided within the STM32Cube_FW_WB_V1.0.0