2024-10-29 11:15 PM
Hi,
I am using Zigbee_OnOff_Router_NVM to test the opening and closing function of IasZone Server. I found that by default, the notification generated by modifying the status value is 'Report Attributes'. But according to document 'Zigbee Cluster Library', a 'Zone Status Change Notification Command' should be generated.
I also found that if the following code is commented on, it can generate the 'Zone Status Change Notification Command' notification correctly, but the status value will lose persistence.
/* Allocate the attributes */
// if (ZbZclAttrAppendList(zigbee_app_info.iaszone_server_1, zcl_iaszone_server_attr_list, ZCL_ATTR_LIST_LEN(zcl_iaszone_server_attr_list)))
// {
// ZbZclClusterFree(zigbee_app_info.iaszone_server_1);
// return ;
// }
I want to know how to generate 'Zone Status Change Notification Command' notifications while enabling data persistence.
I provided the source code I used.
Thanks
DL_Weng
Solved! Go to Solution.
2024-12-03 05:27 AM
Hi @DL_Weng,
Here is the update about this case :
The Zone Status is only written by the application, and reflects the current zone status from the device.
After reboot, it's expected the application should set this value to the corresponding status from the device itself. There should be no need to persist the value inside the cluster, and the persisted value may not accurately represent the current status of the device after coming back online. This is why the ZCL_ATTR_FLAG_PERSISTABLE flag should not be set using ZbZclAttrAppendList for the ZCL_IAS_ZONE_SVR_ATTR_ZONE_STATUS attribute.
Notification remains working when no persistable flag set at the application side.
Best regards,
Ouadi
2024-11-06 07:30 AM
Hello @DL_Weng,
When using ZbZclAttrAppendList API from the application side, it overrides the default definition of the attribute already done at the cluster level, this is why the write callback allowing to send Change Status notify is lost.
I have raised an internal ticket N°195832 to analyze this case and hopefully, to add the persistable flag to the attribute without overriding the default configuration.
I will come back to you asap once the ticket is analyzed.
Best regards,
Ouadi
2024-12-03 05:27 AM
Hi @DL_Weng,
Here is the update about this case :
The Zone Status is only written by the application, and reflects the current zone status from the device.
After reboot, it's expected the application should set this value to the corresponding status from the device itself. There should be no need to persist the value inside the cluster, and the persisted value may not accurately represent the current status of the device after coming back online. This is why the ZCL_ATTR_FLAG_PERSISTABLE flag should not be set using ZbZclAttrAppendList for the ZCL_IAS_ZONE_SVR_ATTR_ZONE_STATUS attribute.
Notification remains working when no persistable flag set at the application side.
Best regards,
Ouadi
2024-12-18 02:39 AM
Interesting discussion!
When I comment this part of code. Device send 'Zone Status Change Notification Command'. Also another thing happen, when after reboot device, no notification sent to Home assistant. It seems device is not successfully add to the network or not send correct command as expected.
/* Allocate the attributes */
// if (ZbZclAttrAppendList(zigbee_app_info.iaszone_server_1, zcl_iaszone_server_attr_list, ZCL_ATTR_LIST_LEN(zcl_iaszone_server_attr_list)))
// {
// ZbZclClusterFree(zigbee_app_info.iaszone_server_1);
// return ;
// }