2019-10-22 7:22 AM
Hello,
I' trying to update the FUS on my STM32WB55CG (1M), I have the latest STM32Cube_FW_WB_V1.3.0, I followed the Release_Notes in the STM32WB_Copro_Wireless_Binaries :
for information I use this chip on my own board (not a nucleo)
I switched the MCU in bootloader
then
then
STEP 4 : Read and upgrade FUS Version
so I need to update it
STEP 5 : Download new FUS :
in my case
STM32_Programmer_CLI.exe -c port=usb1 -vb 2 -fwupgrade stm32wb5x_FUS_fw.bin 0x080EC000 firstinstall=0
I increse the verbose mode to 2 (I join the log file flash_FUS_VB2)
most of the time the upgrade fail during the reconnecting process after Deleting firmware...
if this part pass I have a firmware not authentic at the end
Reconnecting...
Reconnected
Reconnected !
sending an abort request
setting the address pointer to address: 0xffff0054
sending an abort request
FUS state is FUS_UPGRADE_ONGOING
FUS status is FUS_IMAGE_NOT_AUTHENTIC
Error: Firmware not authentic!
and obviously because of this I can't upload the BLE stack.
Your help would be really appreciate, we have a nice project based on this and we would like move forward on this topic.
regards,
Benjamin
2019-10-23 3:45 AM
Hi, Benjamin.
In AN5185, "Table 1" is written:
If an STM32WB5xG device has FUS V1.0.1, then there is no need to upgrade to V1.0.2, since it does not bring any new feature/change vs. V1.0.1.
In case FUS V1.0.2 installation is started by user on an STM32WB5xG device with FUS V1.0.1, FUS returns FUS_STATE_IMG_NOT_AUTHENTIC error and discard the upgrade.
Best regards,
Vyacheslav.
2019-10-23 3:52 AM
Hello Vyacheslav,
I agree with you but in my case the stm32wb55cg has FUSv0.5.3 installed, and I have this problem when I try to upgrade in FUS1.0.1.
regards,
Benjamin
2019-10-23 4:04 AM
Oh, sorry.
It happens to me too.
I try to fill in the FUS several times with the firstinstall value I set it to 0 or to 1.
But I did not notice the logic when a successful update occurs.
2019-10-23 4:14 AM
I also selected 0 then 1 but the result is :
if firstinstall is 1 :
most of the time the upgrade fail during the reconnecting process after Deleting firmware.
if firstinstall is 0:
FUS status is FUS_IMAGE_NOT_AUTHENTIC
Error: Firmware not authentic!
2019-10-23 4:23 AM
How about to try to load FUS ver 1.0.1 from SDK 1.1.0 ?
2019-10-23 4:24 AM
Good idea, I gonna try !
2019-10-23 7:08 AM
It worked, but I'm not comfortable to understand why, and I would do this only on one board I don't have more in provious version anymore
2019-10-23 8:24 AM
It’s the same with me.
After I put the fus 1.0.1, I don’t touch it anymore :)
It seems to me, that this is due to the first revisions of stones that have some kind of glitches.
2019-11-13 10:59 PM
Finally I understood my problem, the boot pin SHALL be pull to VDD during ALL the update