2024-07-04 5:40 AM
I got the STM32W55 MCU.
We keep receiving an event from the stack:
Event type: 0xff -->
HCI_VENDOR_SPECIFIC_DEBUG_EVT_CODE
Event e-code: 0x04
/* ACI_HAL_END_OF_RADIO_ACTIVITY_EVENT code */
#define ACI_HAL_END_OF_RADIO_ACTIVITY_VSEVT_CODE 0x0004U
We receive it in an infinite loop.
Can you please advice?
Solved! Go to Solution.
2024-07-08 8:32 AM
Hello @ezza23
Hi Ezza,
This event is triggered because most probably in your code you registered to receive radio_activity_event ( By default it is the case in ST code example)
To register to radio activity event, I suppose you have a call to aci_hal_set_radio_activity_mask()
This command allow to define radio activity report you want to receive.
If you don't want to receive such report ( ACI_HAL_END_OF_RADIO_ACTIVITY_VSEVT_CODE). You simply need to remove call to aci_hal_set_radio_activity_mask().
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-04 7:29 AM
Hello @ezza23 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Can you give more details about your exact configurations to reproduce this behavior.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-05 2:28 PM
Hi @ezza23
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2024-07-08 8:32 AM
Hello @ezza23
Hi Ezza,
This event is triggered because most probably in your code you registered to receive radio_activity_event ( By default it is the case in ST code example)
To register to radio activity event, I suppose you have a call to aci_hal_set_radio_activity_mask()
This command allow to define radio activity report you want to receive.
If you don't want to receive such report ( ACI_HAL_END_OF_RADIO_ACTIVITY_VSEVT_CODE). You simply need to remove call to aci_hal_set_radio_activity_mask().
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.