2021-01-04 12:10 AM
Hi,
The Ram_Shared address in the linker from cubeMx is 0x20008000 but I think it should be 0x20030000.
Changing this also fixed communications with cpu2 for me.
Solved! Go to Solution.
2021-02-11 12:18 AM
This issue will be solved in the next STM32CubeIDE, Version: 1.6.0 release.
2021-01-04 04:15 AM
Thanks for spotting this issue. I forwarded your findings to the Tools team.
2021-01-11 06:24 AM
Could you send us the erroneous file and tell us which IDE you are using?
We are not able to find it.
2021-01-11 07:19 AM
2021-02-09 02:41 AM
I faced the same issue (STM32CubeIDE v1.5.1 Build: 9029_20201210_1234 (UTC)).
This should be fixed as soon as possible. Otherwise the BLE part of the STM32WB30 is not usable for new customers (at least with the CubeIDE).
As a side note:
It is also neither possible to update the FUS of the STM32WB30 to v1.1.0 nor the BLE stack to v1.10.0 (with the preinstalled FUS).
I first had to get v1.10.1 from github and update FUS to v1.1.2 before I was able to update the BLE stack to v1.10.0 (with the STM32CubeProgrammer v2.6.0).
Thanks for your work & cheers
2021-02-11 12:18 AM
This issue will be solved in the next STM32CubeIDE, Version: 1.6.0 release.