cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB10CC RF output stage design question

77volatile77
Associate

Hello, 

For a personal project, I am designing a device that receives GPS data and transmits the UTC time information to other devices over BLE. I will also be designing a device that receives the data and displays it. For this, I have chosen the STM32WB10 MCU. I think I have a surface-level knowledge of RF, but I couldn't understand this application schematic in AN5290, page 10:

 

77volatile77_0-1690045960408.png

What I am confused about is the low pass filter at the end. Assuming I connect an antenna to the RF output, how would this device work in RX mode? Perhaps as a result to my inexperience with RF, the antenna being connected to the output of the LPF doesn't make sense to me. The same circuit is also showed in AN5165, page 13. 

Thank you in advance for the advice. 

1 ACCEPTED SOLUTION

Accepted Solutions
Nikita91
Lead II

The RF1 pin is not an output pin, but a RX/TX pin. The antenna is used for both.

The filter works in both directions, but its characteristics are not quite symmetrical, hence the terms input/output. It must be soldered the right way.

View solution in original post

1 REPLY 1
Nikita91
Lead II

The RF1 pin is not an output pin, but a RX/TX pin. The antenna is used for both.

The filter works in both directions, but its characteristics are not quite symmetrical, hence the terms input/output. It must be soldered the right way.