STM32WB09 deepstop mode
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-20 10:13 AM
I'm trying to run a sample PWR_DEEPSTOP_RTC from PWR_DEEPSTOP_RTC, but I'm facing some problems.
The code works correctly, the UC enters deepstop mode and returns to run mode, but when I try to measure the current in PJ2 as described in item 7.1.4 of UM3345, I get 90uA when in deepstop mode and not around 1uA as the datasheet says. (RTC wakeUP, LSi 32k).
I follow this example recipe:
/* The following Wakeup sequence is highly recommended before each entry into Deepstop mode
especially when using more than one wakeup source, this is to not miss any wakeup event.
- Disable all used wakeup sources,
- Clear all related wakeup flags,
- Re-enable all used wakeup sources,
- Enter Deepstop mode.
*/
Is there anything I missed or didn't understand?
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-11 4:41 AM
Yes, I am using the ST example, STM32CubeWB0\Projects\NUCLEO-WB09KE\Examples\PWR.
I was only able to achieve the correct current consumption when I went to the .ioc file in CubeMX under Project Manager -> Code Generator -> HAL Settings and enabled the option "Set all free pins as analog (to optimize power consumption)", which is not enabled by default in the provided example.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-10 12:56 PM
Hello @rlopes
First, are you using the same ST Example or another one based on it.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-11 4:41 AM
Yes, I am using the ST example, STM32CubeWB0\Projects\NUCLEO-WB09KE\Examples\PWR.
I was only able to achieve the correct current consumption when I went to the .ioc file in CubeMX under Project Manager -> Code Generator -> HAL Settings and enabled the option "Set all free pins as analog (to optimize power consumption)", which is not enabled by default in the provided example.