cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB - STM32_WPAN (BLE) with FREERTOS

AbidSulaiman
Associate III

Hello,

I am using CubeMX 5.1 and I am aware that it is not possible to activate FREERTOS when STM32_WPAN is activated. Is there any way to integrate FREERTOS with BLE? Is the feature maybe coming out in the future?

21 REPLIES 21

Just ran into this issue yesterday. 
Doesn't seem like this issue has been solved yet. 

  • Comparing BLE_HeartRate and BLE_HeartRateFreeRTOS is less helpful, because neither uses a 'Custom Template'. 
  • The issue is that 'Server Mode' does not show the 'Custom Template' option when FreeRTOS is enabled. 

@Christophe Arnal wrote:

Hello,

 

There are currently two features under development :

  • BLE/FreeRTOS Heart Rate with support of Stop Mode 2
  • CubeMx BLE/FreeRTOS generation support

 

I don't know when this will be available but the development already started. It should be available in some next release)

 

Regards.


Is the FreeRTOS+BLE code generation available now for a custom BLE service?