cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB dual mode at the same time?

DHoff.2
Associate

Is it possible to use MCUs in the STM32WB line in both Bluetooth LE and Bluetooth Classic modes at the same time? I've seen that it does "dual mode", but not whether it can do both at the same time.

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Remi QUINTIN
ST Employee

​STM32WB is offering a set of low power modes that would not fit with the BLE Classic consumption requirements.

This is why it only targets low energy protocols: BLE, BLE Mesh, Thread, Zigbee, 802.15.4.

Only some dual low energy protocol modes are supported: "BLE + Thread" now and "BLE + 802.15.4" in the coming weeks.

View solution in original post

1 REPLY 1
Remi QUINTIN
ST Employee

​STM32WB is offering a set of low power modes that would not fit with the BLE Classic consumption requirements.

This is why it only targets low energy protocols: BLE, BLE Mesh, Thread, Zigbee, 802.15.4.

Only some dual low energy protocol modes are supported: "BLE + Thread" now and "BLE + 802.15.4" in the coming weeks.