2020-09-17 12:34 PM
Hello,
Can I use STM32WB as master/slave at the same time? Our project requests the product to talk with cell phone and other accessories at the same time.
If so, is there an example I can refer to?
Thank you very much!
2020-09-17 2:01 PM
You should have a look at the BLE_p2pRouter project here: STM32Cube_FW_WB_V1.8.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pRouteur.
In this use case, the STM32WB devive maintains seven simultaneously connections to transfer information from one device to an another remote.
A smartphone application is connected to the STM32WB55 P2P router device allowing the control of six others peripheral STM32WB devices.