cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 and Lora(SX1278) TrueSTUDIO project?

Panagiotis
Associate III

I 'm looking for a 100% working example for my MCU (an STM32F030F4P6) at TrueSTUDIO.

Is there such an example?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5

Probably not.

Likely going to need to find something close, and port. And/or construct in your chosen toolchain.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Panagiotis
Associate III

Ok, even something close would help.

If it's tested and working it 'll be very helpful.

At 433 MHz ? LoRa or LoRaWAN ?

Seem to recall most of ST's LRWAN library examples were for the SX1272 and SX1276 parts. Although I don't think the SX1278 would be significantly different.

If you want something that's drop-n-go look at the hardware/boards the LRWAN software supports out-of-the-box and uses those combinations.

https://www.st.com/en/embedded-software/i-cube-lrwan.html

These things can be ported, but it is not a zero cost exercise.

Beyond that, you could mine github or other open source examples, or use the Semtech libraries more directly, without ST's spin on them.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

At 433 MHz, LoRa not LoRaWAN.

Panagiotis
Associate III

2 months later, I have made some progress...:)

I have managed to make the transmitter work!

BUT it does not work as it should: out of the 100 messages it transmits, the receiver receives only 10 to 15...

I have tried sending them every 2.5 Seconds, then every 10 Seconds, every 30 Seconds, but the result is the same.

(this Lora module I 'm using works fine with Arduino)

I 've also tried changing:

-frequency

-Spreading Factor

-Signal Bandwidth

-Transmission Power

-Coding Rate

-SyncWord

-Preamble Length

Without any result.

I have uploaded my code on github, folders Inc and Src (and the whole project in the zip file, just in case).

(the code is a 'mixture' of codes from here and here)

Any help is welcome.