2023-06-19 10:26 AM - last edited on 2023-07-12 02:48 AM by Amel NASRI
I need your help with the STM 32wb5mmg.
Not sure why power consumption is higher (x2) when VREFBUF is defined as an internal voltage reference.
Is this possible because the Vref+ is connected to the VDD?.
Appreciated if you could help with this
2023-06-21 09:55 AM
The customer's Vref is tied to Vdd on their board
Please see link below that talk about the VREFBUF