2017-08-23 12:02 AM
Hello, currently im using B-L072Z-LRWAN1 send AT command to multitech gateway and server is loriot.io. And i cant get data at the server.
Here some information:
Firmware version B-L072Z-LRWAN1 v1.1.1
AT command:
AT
AT+CFM=0
AT+NJM=0
AT+DADDR=...
AT+NWKSKEY=...
AT+APPSKEY=...
AT+JOIN
AT+NJS=? (response = 1)
AT+SEND=1:0123
OK
txDone rxTimeOut rxTimeOutI cant connect to Multitech gateway.
Any suggestion?
#lora #b-l072z-lrwan12017-08-23 06:14 AM
There is a problem with the sscanf() in the AT+SEND command parsing
https://community.st.com/0D50X00009XkXrMSAV
uint8_t appport; needs to be
uint32_t appport;
See also the rest of that thread for some foundation in the issue.
2017-08-23 08:22 AM
Thank for fast answer Clive One
I will try it tomorrow, but my config above is correct ?
I see when i run AT+JOIN the DADDR,
NWKSKEY, APPSKEY is back to default. Is there something wrong?
2017-08-23 09:57 AM
I'm doing mostly point-to-point communication, I don't have a Gateway to tinker with.