cancel
Showing results for 
Search instead for 
Did you mean: 

Send a single advertise packet

DS.4
Senior II

Is there a way to send a single advertisement packet at a specific moment in code, ( without the mix/max interval time).

I want to disable advertisement.

And control it myself.

3 REPLIES 3
Remi QUINTIN
ST Employee

Could you explain the use case behind?

You can anyhow start the advertising phase with a max interval value and then wait for the “end of radio�? event (RF activity window ) and stop the advertising phase.

This way you have only one advertising window on the 3 channels 37,38 and 39.

DS.4
Senior II

Thanks for the answer.

The reason I am asking is that I would like to keep the same behavior from a previous controller.

Any chance a simpler possibility is available? A one shot? Instead of start stop?

Remi QUINTIN
ST Employee

Unfortunately not. We do not have any API enabling this one shot possibility.