2024-07-03 04:55 AM - edited 2024-07-03 05:42 AM
Hello,
I am using a Nucleo-WBA52CG dev. board as well as an sd shield.
I want to store data from the NUCLEO in the SD card, and be able to read those data with a computer.
The SD card and the stm32WBA should obviously communicate through SPI.
However, the WBA does not have FatFS, nor SDMMC. I suppose that I can use FileX to partially "replace" those elements, but I see myself unable to find anything related to that situation. I suppose that I'll have to check the custom interface, and as I want to use EXFAT, enable it. But from there I'm kind of lost.
Does anyone have a way to do those communications?
Thanks in advance.
Don't hesitate if you need other informations to facilitate your understanding and give me some hints.