2025-02-15 8:04 PM
Hi,
I am evaluating/learning the SBSFU application example on STM32WBA55CG. I have disabled the MCUBOOT_HW_ROLLBACK_PROT and generated the signed confirmed image sbsfu_app_init.bin using the imgtool.exe without the security counter TLV using the below command.
imgtool.exe sign -k root-rsa-2048.pem -S 229376 -e little -H 0x400 --pad-header --align 8 --overwrite-only -v 1.0.0 --confirm --pad sbsfu_app_init.bin
The only change I made to the above command is to remove the "-s auto" and +0 from the version to ensure TLV for the security counter isn't added. However, when I run the application, the image validation fails within the bootutil_tlv_iter_begin as shown below i.e
if (info.it_magic == IMAGE_TLV_PROT_INFO_MAGIC) {// fails with info.it_magic = 0x6907
if (hdr->ih_protect_tlv_size != info.it_tlv_tot) {
return -1;
}
if (LOAD_IMAGE_DATA(hdr, fap, off_ + info.it_tlv_tot, &info,
sizeof(info))) {
return -1;
}
} else if (hdr->ih_protect_tlv_size != 0) {//fails with hdr->ih_protect_tlv_size = 4
return -1;
}
I'd expect hdr->ih_protect_tlv_size to be 0 however it is not. Could someone help/advise to resolve this. Any insights would be appreciated.