cancel
Showing results for 
Search instead for 
Did you mean: 

RSSI on LoRa-E5 vs nucleo-WL55JC1

spa23
Associate III

Hi

i'm just sitting and messing with a few lora boards.

I find that nucleo-WL55JC1 has approx 10dbm RSSI better than seeed LoRa-E5, and that nucleo-WL55JC1 also transmits with a more powerful signal, what is your experience ??

with best regards

1 ACCEPTED SOLUTION

Accepted Solutions
spa23
Associate III

i found the error, it was the clock domain for the one gpio pin that was not right, so the one gpio did not work .. :)

my measurements if anyone could be interested ..

0693W00000NrJXWQA3.pngNucleo is a littel bit better.

View solution in original post

12 REPLIES 12
Andrew Neil
Evangelist III

How, exactly, are you determining that?

What, exactly, do you mean by, "seeed LoRa-E5" - a board? a module?

0693W00000NqYZGQA3.pnghttps://www.seeedstudio.com/LoRa-E5-Wireless-Module-p-4745.html

Antennas are bidirectional - so you'd expect better performance in Rx to be reflected in better Tx.

spa23
Associate III

I'm using the E5 mini Dev-board.

So this: https://www.seeedstudio.com/LoRa-E5-mini-STM32WLE5JC-p-4869.html ?

What happens if you swap antennas between this & the Nucleo?

If the improvement follows the antenna, then you have your answer!

spa23
Associate III

Yes, and I get the same result with both antennas.

Louis AUDOLY
ST Employee

Hello @spa23​ ,

It's difficult to say if this is normal to have around 10 dBm less in reception because we do not compare the same board, and maybe even not the same package.

We can have differences between 2 boards depending of the matching design network so it's difficult to tell you where is located with precision the difference between those two boards.

Regards

spa23
Associate III

i found the error, it was the clock domain for the one gpio pin that was not right, so the one gpio did not work .. :)

my measurements if anyone could be interested ..

0693W00000NrJXWQA3.pngNucleo is a littel bit better.

Thanks for the update.

How does a GPIO pin mis-configuration affect RSSI?

Please mark the solution:

0693W000008y9fZQAQ.png

spa23
Associate III

Because that it was one of the rf switch control pins, so the rf switch never switched.

Aha - that'd do it!