2023-02-13 06:32 AM
Hi,
I started a Circuit/PCB design with STM32WL55CCU (UFQPN48) to work at 433MHz.
I was referred to ST design for low band/Hight power and to AN5457.
But I am style missing for some information:
…..
After making some test with the nucleo board wl55, I cannot find the same range like I had with other RF433 module. It is look like RF circuit is not optimised or …. Is anybody have the same observation?
2024-02-18 12:55 PM
I'm having the same questions about PA output impedance at 433Mhz and I also noticed the L6 discrepancy. Would be nice to have some answers...