cancel
Showing results for 
Search instead for 
Did you mean: 

Required and recommended software for working with STM32WB55

STMDesigner
Associate II

Hi,

 

We have designed a board using STM32WB55 and also ordered evaluation kit. Our company policy requires us to request software, so there is 2-3 week delay until we get it. At the moment I am trying to understand what is the required software to make it possible to program and debug the board.

 

This is what I have come up with so far. If there are things I have missed or could benefit from, please give me some rope here so I can request all the useful software from my IT department!

 

Best regards,

STMDesigner

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @STMDesigner 

The STM32CubeMX and STM32CubeProgammer are embedded on the STM32CubeIDE but it will be a good idea to use the standalone versions. It should be really helpful to use the standalone versions of the STM32CubeMX and the STM32CubeProgarmmer may be needed for some actions (mass erase, Stack and FUS update...). Also, the STM32CubeMonitor-RF. may help you for some RF tests. Finally, you will need to download the STM32CubeWB throw the STM32CubeMX.

PS: make sure to always download and install the last version available for all applications.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @STMDesigner 

The STM32CubeMX and STM32CubeProgammer are embedded on the STM32CubeIDE but it will be a good idea to use the standalone versions. It should be really helpful to use the standalone versions of the STM32CubeMX and the STM32CubeProgarmmer may be needed for some actions (mass erase, Stack and FUS update...). Also, the STM32CubeMonitor-RF. may help you for some RF tests. Finally, you will need to download the STM32CubeWB throw the STM32CubeMX.

PS: make sure to always download and install the last version available for all applications.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrew Neil
Super User

https://www.st.com/en/microcontrollers-microprocessors/stm32wb55rg.html#tools-software

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.