2022-03-01 3:23 PM
I'm working with the STM32wb55ceu MCU which states that it has 512K of flash memory starting from address 0x08000000.
However, I realized that if I compile and run the follow program, it will hard fault when attempting to read the value from flash (line 3)
void main ()
{
uint8_t i = *(uint8_t *)0x0806f18c;
(void)i;
while (1);
}
To my understanding, the flash should end at 0x08080000. and I have confirmed that my flash memory size is 512K by using the st-info utility.
Is there some sort of memory protection I need to disable?
Solved! Go to Solution.
2022-03-01 5:25 PM
0x0806f18c is near the end of the flash.
You're probably reading FLASH that is reserved for the second core (CPU2) handling the wireless functions.
From the datasheet:
2022-03-01 3:41 PM
If you dump the faulting address in the Hard Fault handler, what does it report?
Unwritten FLASH may fail ECC checks
2022-03-01 3:54 PM
Looks like BusFault Status Register contains 0x82 which means BFARVALID is set and PRECISERR
if this is what you were asking
2022-03-01 5:25 PM
0x0806f18c is near the end of the flash.
You're probably reading FLASH that is reserved for the second core (CPU2) handling the wireless functions.
From the datasheet:
2022-03-01 5:26 PM
Read out FLASH_SFR to verify what's reserved for CPU2.
2022-03-01 5:27 PM
Makes sense. I missed that in the data sheet. Thank you.