2023-07-26 10:04 PM
Hi
I am planning to use the BlueNrg module in my project , until I found out that I have to pay for the Qualification fee for using BlueTooth. Not sure if I dont display the logo I dont have to purchase it, or do I have to purchase it even if the logo isnt displayed? Below is the link I was giving.
https://www.bluetooth.com/develop-with-bluetooth/qualification-listing/qualification-listing-fees/
Best Regards
Scott
2023-07-27 3:49 AM
> in my project
Makes it sound like this is personal use only, in which case no fee is needed.
Otherwise, if it's a commercial product, yes.
> A Declaration fee must be paid for any new, changed, used or branded Bluetooth product