cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with USART2 Rx Callback with BLE_p2pServer_ota example

ledi7
Associate III

Hi,

i am using the BLE_p2pServer_ota example with NUCLEOWBA55 and i want transmitt a 20 Byte package over USART2 with DMA in circular mode (19200 Baud). Here as an example, i send 20 bytes every second via HTerm to USART2. BLE advertising (every 2s) is working (but i am not connected to the cellphone app). 

The Rx Callback function is inside p2p_server_app.c and here i want to toggle the blue LED:

/* USER CODE BEGIN FD_LOCAL_FUNCTIONS*/
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
   if(huart->Instance == USART2)	// Rx Callback for USART2
   {
	BSP_LED_Toggle(LED_BLUE);
   }
/* USER CODE END FD_LOCAL_FUNCTIONS*/

But after several transmissions (between 50 and 150) the callback function is no longer called.

Does anyone have an idea what is going wrong?

23 REPLIES 23

Duplicate - merged.


Hi,

I use the example “BLE_p2pServer_ota” with NUCLEO-WBA55 as a template for a project. Once a BLE connection is established with the mobile app, I start sending 20 bytes every 3 seconds via a hyperterminal on USART2 and transmitting it as a notification. The transmission basically works, but after a few transmissions (usually between 5 and 15 transmissions) the HAL_UART_RxCpltCallback function is no longer called. I have tried DMA in normal mode and in circular mode. In circular mode it works a bit longer.

1. in main.c i start the UART2 in DMA receive mode:

 

 

 /*##-2- Put UART peripheral in reception process ###########################*/
  /* Any data received will be stored in "aRxBuffer" buffer : the number max of
     data received is 20 */
  if (HAL_UART_Receive_DMA(&huart2, (uint8_t *)aRxBuffer, RXBUFFERSIZE) != HAL_OK)
  {
    //Transfer error in reception process
    Error_Handler();
  }

 

 

2. in Rx callback function i call the task to send a notification. (This is the same task which is used for button1 in the example)

 

 

/* USER CODE BEGIN 4 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
   if(huart->Instance == USART2)  // Rx Callback for USART2 as soon as 20 bytes received
   {
	   UTIL_SEQ_SetTask( 1<<CFG_TASK_SEND_NOTIF_ID, CFG_SEQ_PRIO_0);
   }
}
/* USER CODE END 4 */

 

 

The task was called a few times but never longer as 15 times. 

How can i solve this problem?

 

STTwo-32
ST Employee

Hello @ledi7 

This is not a normal behavior. Could you please try to reproduce it on a simple Code (not inside the Example).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I have created a new project from scratch and i am using USART2 with GPDMA in non-circular and circular mode. Also using 20 byte packets with 19200 baud and everything works fine.

 

So, try to check in case the problem appears if the reception is really ended or not.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

 Yes, but now only under the account ledi7

So we could merge that other thread into this, then?

It's the same question?


Now merged.

Hi,

now i moved the Rx callback function to main.c

/* USER CODE BEGIN 4 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
	if(huart->Instance == USART2)	// Rx Callback for USART2
	{
		BSP_LED_Toggle(LED_BLUE);

		if (HAL_UART_Receive_DMA(&huart2, rxBuffer, RXBUFFERSIZE) != HAL_OK)
		{
			Error_Handler();
		}
	}
}

and i insert also the UART error handling within void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart) Function. 

I occasionally get frame errors here. But when I use my own written program with USART2 DMA functionality only, everything works fine. It seems that something is interfering with the BLE_p2pServer_ota.