cancel
Showing results for 
Search instead for 
Did you mean: 

Problem flashing a card STM32WBA55G

Clemint
Associate II

Hi, 

 

I have a STM32WBA55G card and I want to flash an example code but it doesn't work. So I used STM32Programmer to find out why my board wasn't "found". Normally STLink is included and I can go through the usb-c port. But I still get an error if I go through the uart connection: "Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again... »

Et j’ai toujours l’erreur suivante si je passe par stlink : « Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication »

I can't find the solution, can you help me?

 

Best regards

1 ACCEPTED SOLUTION

Accepted Solutions

Hi, I found the solution. I'm sorry for the inconvenience.

 

I checked every pin. And I noticed that the jumper was badly positioned on the JP5. Sorry for the inconvenience.

 

Kind regards

 

Discovery kit with STM32WBA55CG MCU - User manual

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @Clemint and welcome to the ST Community .

Could you check the following point:
- The USB to micro used is a data transfer and not a simple charging cable?
- JP4 is in position on 5v_STLK? 

Best Regards.

STTwo32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi, 

Yes it is good for these 2 points. 

Best regards

Hi, I found the solution. I'm sorry for the inconvenience.

 

I checked every pin. And I noticed that the jumper was badly positioned on the JP5. Sorry for the inconvenience.

 

Kind regards

 

Discovery kit with STM32WBA55CG MCU - User manual