cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-WL55JC as gateway

KYZ
Associate III

Hello,

 

I'm using Nucleo-WL55JC cards and I wanted to know if it was possible to use them as gateways, partly to connect the radio world to the internet (LoRaWAN), and partly to extend the range of my network (by dispersing multiple gateways everywhere).

Note: there would only be a single "sensor" device that would send its data to the nearest gateway. This "sensor" device is also a Nucleo-WL55JC.

 

Thanks in advance.

 

Best regards,

 

KYZ.

14 REPLIES 14

Thanks for these links! I'll have a look at them.


In fact, I'm looking for as much information as possible to help me with my project.
I'm mainly trying to understand how LoRaWAN works, and also to understand how to set up a LoRa network or use a network already in place, and so on.
I don't want to get into this without understanding how LoRa and LoRaWAN work, so I'm looking for LOTS of information on the subject and that's how new questions come up.
Which may be confusing for you.

KYZ
Associate III

And as far as tracking is concerned, I use a GPS module directly with my device and I want to send this location data to the server.

Hello @KYZ 

I think @Andrew Neil give you resources that should help you. If you still have more questions, you can ask them on a new thread with details if possible. If this post is answered, you may close it by selecting the comment that answer this question as best answer.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@KYZ Indeed, as @STTwo-32 says, I think your question, "Can Nucleo-WL55JC cards be use them as gateways" has been answered.

In summary:

  1. In the specific case of "LoRaWAN Gateway" (capital 'G' - Proper Name) as defined in the LoRaWAN specifications: No, a WL55 cannot do that.
     
  2. In the generic sense of "gateway" (small 'g'), yes it could be possible for a WL55 to be both an End Node in a LoRaWAN and also participate in some other network - thus providing a "gateway" (in the generic sense) or "bridge" between the two.
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi @Andrew Neil 

I only see your answer now, sorry
Thank you for your reply !

Bests regards

KYZ.