2021-01-06 11:48 PM
Have built the (single core) LoRaWAN AT Slave example from STM32Cube_FW_WL_V1.0.0, which has been flashed to a new Nucleo STM32WL55 board (straight out of the package). No apparent problems building and flashing. Configured for AS923 region.
Running an OTAA Join command the terminal returns:
AT+JOIN=1
35s069:TX on freq 923400000 Hz at DR 2
OK
35s461:MAC txDone
40s447:RX_1 on freq 923400000 Hz at DR 2
40s523:MAC rxTimeOut
41s447:RX_2 on freq 923200000 Hz at DR 2
41s523:MAC rxTimeOut
+EVT:JOIN FAILED
Looks ok but problem is that the radio isn't transmitting at all, as checked with a spectrum analyser (which sees output from other LoRaWAN boards running that frequency band).
Could be a simple configuration problem, but everything looks ok.
Suggestions would be welcome?
Solved! Go to Solution.
2021-01-07 02:22 PM
Oh Oh!
Answer to this question is that I have the low frequency version of the Nucleo board!! It does transmit but output is of course very weak at around 923MHz.
Darn. Have just ordered the correct board.
2021-01-07 02:22 PM
Oh Oh!
Answer to this question is that I have the low frequency version of the Nucleo board!! It does transmit but output is of course very weak at around 923MHz.
Darn. Have just ordered the correct board.