Not Receiving UART message from STM32WL5M to Laptop
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 1:41 AM - last edited on ‎2025-02-11 6:17 AM by Andrew Neil
Hi there, I have an B-WL5M-SUBG1 evaluation board which uses the STM32WL5M module.
I am having problems with the STM32 receiving a message I am sending it from my laptop via python.
I connect between the stm32 and the laptop via an RS422/485 converter. I've used the converter many times before to read print statements from the stm32.
Here is the stm32 code I am using:
#include "main.h"
#include "stm32wlxx_hal.h"
#include <string.h>
#include <stdio.h>
/* Private variables */
UART_HandleTypeDef huart2;
uint8_t rx_buffer[4]; // Buffer for received data
volatile uint8_t data_received = 0; // Flag for data reception
/* Function prototypes */
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
void Error_Handler(void);
void check_uart_errors(void);
int main(void)
{
uint8_t tx_ready[] = "READY\r\n";
/* Initialize system */
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
/* Reset UART2 before use */
__HAL_RCC_USART2_FORCE_RESET();
HAL_Delay(10);
__HAL_RCC_USART2_RELEASE_RESET();
MX_USART2_UART_Init();
/* Transmit READY message */
if (HAL_UART_Transmit(&huart2, tx_ready, sizeof(tx_ready) - 1, 300) != HAL_OK)
{
Error_Handler();
}
HAL_Delay(10); // Prevent issues
/* Clear UART RX buffer and start receiving */
__HAL_UART_FLUSH_DRREGISTER(&huart2);
memset(rx_buffer, 0, sizeof(rx_buffer));
if (HAL_UART_Receive_IT(&huart2, rx_buffer, sizeof(rx_buffer)) != HAL_OK)
{
Error_Handler();
}
while (1)
{
if (data_received)
{
data_received = 0; // Reset flag
/* Debug: Print received bytes */
char debug_msg[50];
sprintf(debug_msg, "RX CALLBACK: %02X %02X %02X %02X\r\n",
rx_buffer[0], rx_buffer[1], rx_buffer[2], rx_buffer[3]);
HAL_UART_Transmit(&huart2, (uint8_t *)debug_msg, strlen(debug_msg), 300);
HAL_Delay(10);
/* Echo back the received 4 bytes */
if (HAL_UART_Transmit(&huart2, rx_buffer, 4, 300) != HAL_OK)
{
Error_Handler();
}
/* Restart reception */
memset(rx_buffer, 0, sizeof(rx_buffer));
if (HAL_UART_Receive_IT(&huart2, rx_buffer, sizeof(rx_buffer)) != HAL_OK)
{
Error_Handler();
}
check_uart_errors(); // Check for errors after transmission
}
}
}
/**
* @brief System Clock Configuration
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6; // 4 MHz
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK |
RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief USART2 Initialization Function
*/
static void MX_USART2_UART_Init(void)
{
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief UART RX Complete Callback
*/
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if (huart->Instance == USART2)
{
data_received = 1; // Set flag to process received data
}
}
/**
* @brief Check UART Errors
*/
void check_uart_errors(void)
{
uint32_t error = HAL_UART_GetError(&huart2);
if (error != HAL_UART_ERROR_NONE)
{
char error_msg[50];
sprintf(error_msg, "UART ERROR: 0x%lX\r\n", error);
HAL_UART_Transmit(&huart2, (uint8_t *)error_msg, strlen(error_msg), 300);
}
}
/**
* @brief GPIO Initialization Function
*/
static void MX_GPIO_Init(void)
{
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Configure PA2 and PA3 as Alternate Function (AF7) for USART2 */
GPIO_InitStruct.Pin = GPIO_PIN_2 | GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
/**
* @brief Error Handler.
*/
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
My python code is this:
#!/usr/bin/env python3
import serial
import time
def main():
ser = serial.Serial(
port="COM4",
baudrate=115200,
bytesize=8,
parity='N',
stopbits=1,
timeout=2,
xonxoff=False,
rtscts=False,
dsrdtr=False
)
print(f"Opened COM4 at {ser.baudrate} baud.")
# Wait for READY message
start_time = time.time()
ready_received = False
while time.time() - start_time < 5:
line = ser.readline()
if line:
decoded = line.decode(errors="replace")
print("MCU says:", decoded, end='')
if "READY" in decoded:
ready_received = True
break
if not ready_received:
print("No READY message received from MCU.")
ser.close()
return
# Clear UART buffer before sending
ser.reset_input_buffer()
time.sleep(0.1)
# Send 4 bytes
test_msg = b"DATA"
print("\nSending:", test_msg)
ser.write(test_msg)
ser.flush()
# Wait for response with timeout
timeout = time.time() + 5
while time.time() < timeout:
line = ser.readline()
if line.startswith(b"RX CALLBACK: "):
print("MCU Debug:", line.decode(errors="replace").strip())
continue
elif len(line) == 4:
print("Received:", line)
break
else:
print("Error: No response received from STM32.")
ser.close()
print("Done.")
if __name__ == "__main__":
main()
and my output from python is:
Opened COM4 at 115200 baud.
MCU says: READY
Sending: b'DATA'
Error: No response received from STM32.
Done.
Does anybody have any ideas on what the problem is here and how I could fix it. Any help would be greatly appreciated.
Thank you.
- Labels:
-
STM32WL series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 6:24 AM
Have you tested the code using just a terminal?
Have you used the STM32 debugger to see what (if anything) the MCU actually receives from the PC, and if it thinks it sends anything back?
@Dicko wrote:I connect between the stm32 and the laptop via an RS422/485 converter..
Show the full schematic of this connection
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 6:34 AM - edited ‎2025-02-11 8:32 AM
Hello @Dicko
If you are connecting the B-WL5M-SUBG1 to a RS485 port, you should configure the USART2 on mode RS485. After doing that, please debug the code to see if the message is received or not on the MCU side.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 7:53 AM
Thanks for the advice Neil. I will try this first thing tomorrow. Although I’ve never used the STM32 debugger. I’ll try and figure it out and let you know the results.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 7:54 AM
Thanks for the advice STTwo-32. I’ve been trying to find some information about USART3 for this board but it’s not mentioned in any of the schematics.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 8:03 AM
In this module, there is only 2 USARTs and an LPUART. there is not any other UART IP.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 8:31 AM
Ah, but you said to configure USART3?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 8:33 AM
Is just a typo. I've rectified. Thank you so much.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 9:40 AM
Ah thank you. I set up USART2 as Asynchronous, I guess RS485 is a different option. I’ll look at this tomorrow too. Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-11 9:47 AM
With RS485, you have to deal with enabling/disabling the transmitter.
But you said you're using "an RS422/485 converter" - so maybe that doesn't matter in your case?
That's why you need to give full details of how you have this setup - eg, a schematic.
Is there any particular reason for going RS422/485 ?
A complex system designed from scratch never works and cannot be patched up to make it work.