cancel
Showing results for 
Search instead for 
Did you mean: 

NMI error when running BLE stack 1.13.3 full extended with SRAM2 parity enable

AnthonyS
Associate II

Hello,

I updated my application from the "full" to the "full extended" BLE stack 1.13.3.

I modified the link file as requested in the release note.

My issue is that if I keep the SRAM2 parity enable my application crash in NMI error. When I disable the parity it is OK.

This issue was fixed by with stack 1.13.0 "full" but seems to be back it "full extended" variant.

BR

2 REPLIES 2
Remy ISSALYS
ST Employee

Hello,

You can look the errata sheet ES0394, see the following extract:

0693W00000Nr70zQAB.jpg 

Best Regards

AnthonyS
Associate II

Hello,

Thank you , you are right, I configured the section MB_MEM2 as a no_init section to reduce starting time. It works fine with 1.13.3 full but not with 1.13.3 full extended.

Adding a manual initialization of MB_MEM2 to 0 before starting the core 2 solved my issue.

BR