2020-04-02 08:33 AM
To achieve the +6dBm output power on the WB55, VDD needs to be > 1.95V. What is the max ouput power you can achieve if the device is operated at 1.8V?
2020-04-03 12:55 AM
With SMPS ON, it is required to have VDD > 1V95 to get Pmax = 6dBm.
But with SMPS BYPASS, Pmax = 6 dBm can be achieved with only VDD > 1V71.
We did not test the configuration you ask for: SMPS ON with VDD = 1V8.