cancel
Showing results for 
Search instead for 
Did you mean: 

Manually set Spreading Factor and TX power

helixembedded
Associate II

We're using the STM32WLE5JC to develop a LoRa-based project. We are looking into testing our sensor in a very specific environment with very specific settings - the TX power and Spreading Factor. Can these two be manually configured?

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @helixembedded 

Yes, you can change those two parameters on the "subghz_phy_app.h" file of your project:

STTwo32_0-1729248035796.png

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @helixembedded 

Yes, you can change those two parameters on the "subghz_phy_app.h" file of your project:

STTwo32_0-1729248035796.png

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.