2024-10-16 8:56 PM
Hello ,
what is maximum data transmission and reception size (buffer size allowed ) using 434Mhz frequency ?? also what is sync word and preamble setting and encoding mechanism used in controller
any one know details about this please let me know
Solved! Go to Solution.
2024-10-18 3:19 AM
Hello @pooja
1. Maximum data rate: 300 2(G)FSK[kbit/s] and 600 4(G)FSK[kbit/s].
2. The payload size corresponds to the PCKTLEN value. It can be from 0 to 65535 bytes.
3. For Sync word, preamble setting and encoding mechanism see RM0511 chapter 29.3.1.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-18 3:19 AM
Hello @pooja
1. Maximum data rate: 300 2(G)FSK[kbit/s] and 600 4(G)FSK[kbit/s].
2. The payload size corresponds to the PCKTLEN value. It can be from 0 to 65535 bytes.
3. For Sync word, preamble setting and encoding mechanism see RM0511 chapter 29.3.1.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.