cancel
Showing results for 
Search instead for 
Did you mean: 

LoRa end node and gateway with NUCLEO-WL55JC1.

AChud.3
Associate

Hi,

I have two NUCLEO-WL55JC1 boards with me. I want to make one board as a end device and one board as a gateway. I found end node example with in firmware package of STM32WL but not found any example for gateway.

Is there any gateway example available for NUCLEO-WL55JC1?

Is this board(NUCLEO-WL55JC1) capable to run gateway example on it?

Please help me to resolve above questions.

Thanks,

Ankit

1 REPLY 1
Bruno_ST
ST Employee

Hello @Community member​ 

The STM32WL55 is a the device is radio based on Semtech SX126x. The 'commercial' gateway as usually based on SX1301. I am not aware of a projet supporting shield with Wifi/Ethernet to allow NUCLEO-WL55JC1 to become a 'single channel LoRa gateway' as packet forwarder like I-NUCLEO-LRWAN1 LoRa® HF band (868/915/923 MHz) sensor expansion board (https://www.st.com/en/evaluation-tools/p-nucleo-lrwan2.html) based on the STM32L052 MCU + Semtech SX1272 transceiver.

Hoewer, there is a ping/pong example to allow communication between your two STM32WL nucleos.

BR,

Bruno

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.