2021-12-16 11:40 PM
2022-04-12 02:21 AM
Hello,
Only a few examples are using an RTOS. Indeed, most of our examples are using the sequencer which behaves like a ‘bare metal’. You can look directly to the following files stm32_seq.h inside the following folder Firmware\Utilities\sequencer to get the description of the sequencer which can be considered somehow as an “advanced bare metal�? implementation.
Best Regards