2021-07-19 7:12 AM
Is it possible to integrate BLE OTA functionalities into BLE LLD projects? For example, we would like to make the BLE_LLD_Proximity example OTA compatibile, which however requires the FW stm32wb5x_BLE_LLD_fw.bin, while the BLE Ota bootloader example requires the FW stm32wb5x_BLE_Stack_full_fw.bin to work. Or is there a Ble Ota LLD example project that works with FW stm32wb5x_BLE_LLD_fw.bin? Any help is greatly appreciated, thank you.
2021-08-10 8:29 AM
No there will be no integration of this BLE OTA functionality in any of the BLE LLD projects.
BLE OTA is functional with the current BLE stack to transfer and install a binary file.
You can use the BLE OTA example and try to reproduce it with the transport layer BLE LLD to LLD OTA.
Note that FUS will have to be used to install a new FW version.