cancel
Showing results for 
Search instead for 
Did you mean: 

IEEE 802.15.4 BEACON Mode

MYous.3
Associate II

Hello ST Community​,

I want to know if the STM32WB55RG supports MAC 802.15.4 Beacon Mode.

For now, I'm sure that the CM0+ Stack supports Only the Non Beacon Mode (SO=BO=15) and Full broadcast Mode (PANID 0xFFFF​, dest @ 0xFFFF) and OFC doesn't support PIB security model defined by the standard.

I have tried to enable the Beacon mode but no luck.

I always end up with a 0xC0 status when trying to send Data and my sniffer catches nothing ( no beacons are sent nor Data ).

Can somebody please confirm that the Stack doesn't support Beacon Mode ?

Regards,​

1 REPLY 1
Remy ISSALYS
ST Employee

Hello,

You are right, the 802_15_4 beacon mode is not supported on STM32WB.

Best Regards