2020-05-13 11:12 AM
2020-05-13 11:22 AM
The radio can receive the signals, you'd have to own the task of writing the gateway functionality.
It is not well suited to dealing with multiple nodes transmitting at random times, and on top of each other.
2020-05-13 12:18 PM
A pair of B-L072Z-LRWAN can be used in a point-to-point mode, more could broadcast one-to-many.
For a gateway class device look at https://www.st.com/en/evaluation-tools/p-nucleo-lrwan3.html
2020-05-13 01:56 PM
Can I have two B-L072Z-LRWAN talking to each other?
2020-05-13 02:23 PM
Yes, like I said point-to-point
The ping-pong example alternates, but you could just as easily have a committed transmitter, and a committed receiver, and send GPS coordinates and temperature measurements, for example